Solution
Fitness Equipment and Machines
A fitness machine manufacturer wants multiple load measurement systems for their different fitness machines such as the elliptical, leg press, rowing machine, and the cable machine.
A fitness machine manufacturer wants multiple load measurement systems for their different fitness machines such as the elliptical, leg press, rowing machine, and the cable machine. They want to ensure the machines functioning properly to prevent injuries. It can also be used for trainers who want to conduct strength and endurance tests.
A combination of products such as the WMCFP Overload Protected Sealed Stainless Steel Miniature Load Cell, SSB Sealed Beam Load Cells, and AT103 Axial Torsion Force and Torque Transducers. Paired with Interface’s proper instrumentation, the forces can be measured, graphed, and displayed during the testing stage.
Interface’s products all effectively measured forces needed for those working out or undergoing athletic training. Not only did it ensure the machines were working properly, but it also helped those using them to track their endurance performance.
Notifications